This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6746主频最高多少?

Other Parts Discussed in Thread: TMS320C6746

       TI 工程师,现在C6746主频配置为300MHz,看TI  TMS320C6746 DSP Technical Reference Manual

文献 可以将DSP的芯片最高配置为600Mhz,请问下,C6746最高主频能做到600MHz吗?

       另外,想提高DSP 和FPGA之间的读写数据时间,现在测试大概每读一次或者写一次时间为350ns,

读写时间最短可以配置为多长?

  • #1. 芯片主频有2种型号,375MHz,和456MHz。根据芯片手册7.1.2 Device Nomenclature对照你手头芯片的marking看是什么主频的。

    300MHz是大概silicon 1.1时的规格了吧,后面的新版本芯片已经统一提高了主频,没有300MHz这个版本了。

    #2。 EMIFA的速度,一方面由EMIFA的时钟频率决定,参考数据手册的Table 6-5, 最高可配置到148MHz。

        另一方面是根据外面接的芯片的时序要求配置setup, strobe, hold参数,都配置0,则每个阶段为1个EMIFA时钟周期,这是取决于外面的芯片能否接受这么快的速度,而不是EMIFA的限制了。