TI 工程师,现在C6746主频配置为300MHz,看TI TMS320C6746 DSP Technical Reference Manual
文献 可以将DSP的芯片最高配置为600Mhz,请问下,C6746最高主频能做到600MHz吗?
另外,想提高DSP 和FPGA之间的读写数据时间,现在测试大概每读一次或者写一次时间为350ns,
读写时间最短可以配置为多长?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI 工程师,现在C6746主频配置为300MHz,看TI TMS320C6746 DSP Technical Reference Manual
文献 可以将DSP的芯片最高配置为600Mhz,请问下,C6746最高主频能做到600MHz吗?
另外,想提高DSP 和FPGA之间的读写数据时间,现在测试大概每读一次或者写一次时间为350ns,
读写时间最短可以配置为多长?
#1. 芯片主频有2种型号,375MHz,和456MHz。根据芯片手册7.1.2 Device Nomenclature对照你手头芯片的marking看是什么主频的。
300MHz是大概silicon 1.1时的规格了吧,后面的新版本芯片已经统一提高了主频,没有300MHz这个版本了。
#2。 EMIFA的速度,一方面由EMIFA的时钟频率决定,参考数据手册的Table 6-5, 最高可配置到148MHz。
另一方面是根据外面接的芯片的时序要求配置setup, strobe, hold参数,都配置0,则每个阶段为1个EMIFA时钟周期,这是取决于外面的芯片能否接受这么快的速度,而不是EMIFA的限制了。