This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

8168 数据格式



你好,FPGA+8168,FPGA发送模式BT1120,逐行模式,8168收到后的数据地址是是不是Field 0 Y -> addr[0][0], Field 1 Y -> addr[1][0]
Field 0 U -> addr[0][1], Field 1 U -> addr[1][1]    Field 0 V -> addr[0][2], Field 1 V -> addr[1][2]。


Field 0 Y大小:1920*540

Field 1 Y大小:1920*540

Field 0 U大小:1920*540

Field 1 U大小:1920*540

Field 0 V大小:1920*540

Field1  V大小:1920*540