This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于从CCS3.3 迁移到CCS5.5 出现的问题



1. 用CCS5.5 编译后发现 TIMER_TCR_IDLEEN_DEFAULT  在头文件中就找不见  定位不到指定的头文件,请问我将如何修改工程,(还需要设置哪些东西)才能保证与CCS3.3生成的工程文件一样。  

#define TIMER_CTRL    TIMER_TCR_RMK(\
                      TIMER_TCR_IDLEEN_DEFAULT,    /* IDLEEN == 0 */ \
                      TIMER_TCR_FUNC_OF(0),        /* FUNC   == 0 */ \
                      TIMER_TCR_TLB_RESET,         /* TLB    == 1 */ \
                      TIMER_TCR_SOFT_BRKPTNOW,     /* SOFT   == 0 */ \
                      TIMER_TCR_FREE_WITHSOFT,     /* FREE   == 0 */ \
                      TIMER_TCR_PWID_OF(0),        /* PWID   == 0 */ \
                      TIMER_TCR_ARB_RESET,         /* ARB    == 1 */ \
                      TIMER_TCR_TSS_START,         /* TSS    == 0 */ \
                      TIMER_TCR_CP_PULSE,          /* CP     == 0 */ \
                      TIMER_TCR_POLAR_LOW,         /* POLAR  == 0 */ \
                      TIMER_TCR_DATOUT_0           /* DATOUT == 0 */ \
)

2.C5509_UART工程中   

   在CCS5.5 中   ioport unsigned int *PCR_1=(unsigned int *)0x2c12;         ioport 关键字 提示有问题 ,如何在CCS5.5 中解决?
工程见附件。谢谢
C5509_UART.rar