CCSTUDIO: CCS编译器怎样设置生成的烧录文件不包含BOOT_RSVD内容

Part Number: CCSTUDIO
Other Parts Discussed in Thread: TMS320F280039

之前发的贴子是询问C2Prog烧录TMS320F280039芯片报故障的原因。后面查找对比HEX文件,发现多了一段放在RAM地址的内容。这段是由CMD里BOOT_RSVD开辟的地址。

请问如何将BOOT_RSVD生成内容不包含在烧录文件中,我将BOOT_RSVD定义注释掉还是有数据生成放在RAM中

  • 您好,收到了您的案例,调查需要些时间,感您的耐心等待。

  • 您好,

    引导 ROM 堆栈使用 BOOT_RSVD 段。

    相关主题:BOOT_RSVD usage

    如果您不希望在链接器命令文件中包含 BOOT_RSVD 段、那么是的,您应该将其注释掉。

  • 我注释掉,但是代码依然存在,只是存放的位置变了

    帮忙看下我的CMD文件是不是有问题

    /*
    //###########################################################################
    //
    // FILE: F280039_flash_lnk.cmd
    //
    // TITLE: Linker Command File For F280039 Device
    //
    //###########################################################################
    */
    MEMORY
    {

    //BOOT_RSVD : origin = 0x00000002, length = 0x00000126

    RAMM0 : origin = 0x00000128, length = 0x000002D8
    //RAMM1 : origin = 0x00000400, length = 0x000003F8 /* on-chip RAM block M1 */
    //RAMM1_RSVD : origin = 0x000007F8, length = 0x00000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

    RAMLS0 : origin = 0x00008000, length = 0x00003800
    //RAMLS1 : origin = 0x00008800, length = 0x00000800
    // RAMLS2 : origin = 0x00009000, length = 0x00000800
    // RAMLS3 : origin = 0x00009800, length = 0x00000800
    // RAMLS4 : origin = 0x0000A000, length = 0x00000800
    // RAMLS5 : origin = 0x0000A800, length = 0x00000800
    // RAMLS6 : origin = 0x0000B000, length = 0x00000800
    RAMLS7 : origin = 0x0000B800, length = 0x00000800

    /* Combining all the LS RAMs */
    //RAMLS : origin = 0x00008000, length = 0x00004000

    RAMGS0 : origin = 0x0000C000, length = 0x00003FF8
    // RAMGS1 : origin = 0x0000D000, length = 0x00001000
    // RAMGS2 : origin = 0x0000E000, length = 0x00001000
    // RAMGS3 : origin = 0x0000F000, length = 0x00000FF8
    //RAMGS3_RSVD : origin = 0x000FFF8, length = 0x00000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

    BOOTROM : origin = 0x003F8000, length = 0x00007FC0
    SECURE_ROM : origin = 0x003F2000, length = 0x00006000

    RESET : origin = 0x003FFFC0, length = 0x00000002

    #ifdef __TI_COMPILER_VERSION__
    #if __TI_COMPILER_VERSION__ >= 20012000
    GROUP { /* GROUP memory ranges for crc/checksum of entire flash */
    #endif
    #endif
    BEGIN : origin = 0x00080000, length = 0x00000002
    /* Flash sectors */
    /* BANK 0 */
    FLASH_BANK0_SEC0 : origin = 0x080002, length = 0x00FFFE
    /*
    FLASH_BANK0_SEC1 : origin = 0x081000, length = 0x001000
    FLASH_BANK0_SEC2 : origin = 0x082000, length = 0x001000
    FLASH_BANK0_SEC3 : origin = 0x083000, length = 0x001000
    FLASH_BANK0_SEC4 : origin = 0x084000, length = 0x001000
    FLASH_BANK0_SEC5 : origin = 0x085000, length = 0x001000
    FLASH_BANK0_SEC6 : origin = 0x086000, length = 0x001000
    FLASH_BANK0_SEC7 : origin = 0x087000, length = 0x001000
    FLASH_BANK0_SEC8 : origin = 0x088000, length = 0x001000
    FLASH_BANK0_SEC9 : origin = 0x089000, length = 0x001000
    FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000
    FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000
    FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000
    FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000
    FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000
    FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x001000*/

    /* BANK 1 */
    FLASH_BANK1_SEC0 : origin = 0x090000, length = 0x010000
    /*
    FLASH_BANK1_SEC1 : origin = 0x091000, length = 0x001000
    FLASH_BANK1_SEC2 : origin = 0x092000, length = 0x001000
    FLASH_BANK1_SEC3 : origin = 0x093000, length = 0x001000
    FLASH_BANK1_SEC4 : origin = 0x094000, length = 0x001000
    FLASH_BANK1_SEC5 : origin = 0x095000, length = 0x001000
    FLASH_BANK1_SEC6 : origin = 0x096000, length = 0x001000
    FLASH_BANK1_SEC7 : origin = 0x097000, length = 0x001000
    FLASH_BANK1_SEC8 : origin = 0x098000, length = 0x001000
    FLASH_BANK1_SEC9 : origin = 0x099000, length = 0x001000
    FLASH_BANK1_SEC10 : origin = 0x09A000, length = 0x001000
    FLASH_BANK1_SEC11 : origin = 0x09B000, length = 0x001000
    FLASH_BANK1_SEC12 : origin = 0x09C000, length = 0x001000
    FLASH_BANK1_SEC13 : origin = 0x09D000, length = 0x001000
    FLASH_BANK1_SEC14 : origin = 0x09E000, length = 0x001000
    FLASH_BANK1_SEC15 : origin = 0x09F000, length = 0x001000*/

    /* BANK 2 */
    FLASH_BANK2_SEC0 : origin = 0x0A0000, length = 0x00FFF0
    /*
    FLASH_BANK2_SEC1 : origin = 0x0A1000, length = 0x001000
    FLASH_BANK2_SEC2 : origin = 0x0A2000, length = 0x001000
    FLASH_BANK2_SEC3 : origin = 0x0A3000, length = 0x001000
    FLASH_BANK2_SEC4 : origin = 0x0A4000, length = 0x001000
    FLASH_BANK2_SEC5 : origin = 0x0A5000, length = 0x001000
    FLASH_BANK2_SEC6 : origin = 0x0A6000, length = 0x001000
    FLASH_BANK2_SEC7 : origin = 0x0A7000, length = 0x001000
    FLASH_BANK2_SEC8 : origin = 0x0A8000, length = 0x001000
    FLASH_BANK2_SEC9 : origin = 0x0A9000, length = 0x001000
    FLASH_BANK2_SEC10 : origin = 0x0AA000, length = 0x001000
    FLASH_BANK2_SEC11 : origin = 0x0AB000, length = 0x001000
    FLASH_BANK2_SEC12 : origin = 0x0AC000, length = 0x001000
    FLASH_BANK2_SEC13 : origin = 0x0AD000, length = 0x001000
    FLASH_BANK2_SEC14 : origin = 0x0AE000, length = 0x001000
    FLASH_BANK2_SEC15 : origin = 0x0AF000, length = 0x000FF0*/
    //FLASH_BANK2_SEC15_RSVD : origin = 0x0AFFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

    #ifdef __TI_COMPILER_VERSION__
    #if __TI_COMPILER_VERSION__ >= 20012000
    } crc(_table_name, algorithm=C28_CHECKSUM_16)
    #endif
    #endif

    }


    SECTIONS
    {
    codestart : > BEGIN, ALIGN(8)
    .text : >> FLASH_BANK0_SEC0 | FLASH_BANK1_SEC0, ALIGN(8)
    .cinit : > FLASH_BANK2_SEC0, ALIGN(8)
    .switch : > FLASH_BANK2_SEC0, ALIGN(8)
    .reset : > RESET, TYPE = DSECT /* not used, */

    .stack : > RAMLS7

    #if 0 //defined(__TI_EABI__)
    .init_array : > FLASH_BANK0_SEC1, ALIGN(8)
    .bss : > RAMLS5
    .bss:output : > RAMLS3
    .bss:cio : > RAMLS0
    .data : > RAMLS5
    .sysmem : > RAMLS5
    .const : > FLASH_BANK0_SEC4, ALIGN(8)
    #else
    .pinit : > FLASH_BANK0_SEC0, ALIGN(8)
    .ebss : > RAMGS0
    .esysmem : > RAMGS0
    .cio : > RAMGS0
    .econst : > FLASH_BANK0_SEC0, ALIGN(8)
    #endif

    //ramgs0 : > RAMGS0
    //ramgs1 : > RAMGS0

    /* Allocate IQ math areas: */
    IQmath : > FLASH_BANK0_SEC0, ALIGN(8)
    IQmathTables : > FLASH_BANK0_SEC0, ALIGN(8)


    ramfuncs : {} LOAD = FLASH_BANK0_SEC0,
    RUN = RAMLS0,
    LOAD_START(_RamfuncsLoadStart),
    LOAD_SIZE(_RamfuncsLoadSize),
    LOAD_END(_RamfuncsLoadEnd),
    RUN_START(_RamfuncsRunStart),
    RUN_SIZE(_RamfuncsRunSize),
    RUN_END(_RamfuncsRunEnd),
    //ALIGN(8)
    PAGE = 0, ALIGN(8)
    /*
    ramfuncs : LOAD = FLASH_BANK0_SEC0,
    RUN = RAMLS0,
    PAGE = 0
    ALIGN(8)
    table(_prginRAM)
    */
    /* crc/checksum section configured as COPY section to avoid including in executable */
    //.TI.memcrc : type = COPY

    }
    /*
    //###########################################################################
    // End of file.
    //###########################################################################
    */