This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
23.2.4.3.2 Transfers through the DMA Port
CAUTION
To perform internal transfers through the DMA port, clear XBUSEL/RBUSEL bit
to 0 in the respective XFMT/RFMT registers. Failure to do so will result in
software malfunction.
Typically, you will access the McASP XRBUF registers through the DMA port. To access through the DMA
port, simply have the CPU or DMA access the XRBUF through its DMA port location. See your
device-specific data manual for the exact memory address. Through the DMA port, the DMA/CPU can
service all the serializers through a single address. The McASP automatically cycles through the
appropriate serializers.
For transmit operations through the DMA port, the DMA/CPU should write to the same XBUF DMA port
address to service all of the active transmit serializers. In addition, the DMA/CPU should write to the XBUF
for all active transmit serializers in incremental (although not necessarily consecutive) order. For example,
if serializers 0, 4, 5, and 7 are set up as active transmitters, the DMA/CPU should write to the XBUF DMA
port address four times with data for serializers 0, 4, 5, and 7 upon each transmit data ready event. This
exact servicing order must be followed so that data appears in the appropriate serializers.
Similarly, for receive operations through the DMA port, the DMA/CPU should read from the same RBUF
DMA port address to service all of the active receive serializers. In addition, reads from the active receive
serializers through the DMA port return data in incremental (although not necessarily consecutive) order.
For example, if serializers 1, 2, 3, and 6 are set up as active receivers, the DMA/CPU should read from
the RBUF DMA port address four times to obtain data for serializers 1, 2, 3, and 6 in this exact order,
upon each receive data ready event.
When transmitting, the DMA/CPU must write data to each serializer configured as "active" and "transmit"
within each time slot. Failure to do so results in a buffer underrun condition (Section 23.2.4.7.2). Similarly,
when receiving, data must be read from each serializer configured as "active" and "receive" within each
time slot. Failure to do results in a buffer overrun condition (Section 23.2.4.7.3).
To perform internal transfers through the DMA port, clear XBUSEL/RBUSEL bit to 0 in the respective
XFMT/RFMT registers.