This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP6416T



6416T EMIF支持的SDRAM,最高到什么版本,支持DDR2吗

  • EMIF device speed
    The rated EMIF speed, referring to both EMIFA and EMIFB, of these devices only applies to the SDRAM
    interface when in a system that meets the following requirements:
    − 1 chip-enable (CE) space (maximum of 2 chips) of SDRAM connected to EMIF
    − up to 1 CE space of buffers connected to EMIF
    − EMIF trace lengths between 1 and 3 inches
    − 166-MHz SDRAM for 133-MHz operation (applies only to EMIFA)
    − 143-MHz SDRAM for 100-MHz operation

      不支持DDR。