6416T EMIF支持的SDRAM,最高到什么版本,支持DDR2吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
EMIF device speed
The rated EMIF speed, referring to both EMIFA and EMIFB, of these devices only applies to the SDRAM
interface when in a system that meets the following requirements:
− 1 chip-enable (CE) space (maximum of 2 chips) of SDRAM connected to EMIF
− up to 1 CE space of buffers connected to EMIF
− EMIF trace lengths between 1 and 3 inches
− 166-MHz SDRAM for 133-MHz operation (applies only to EMIFA)
− 143-MHz SDRAM for 100-MHz operation
不支持DDR。