This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
我们现在在DM36X平台的IPNC3.1内核下测试SPI,发现在davinci_spi_master.c中配置
iowrite32(0 | (8 << 24) | (08 << 16), davinci_spi->base + SPIDELAY); 编译后,用示波器测量clk, cs信号线,发现 tC2TDELAY 和 tT2CDELAY 总是为0, 理论上应该如图1,图2的波形才对
请问是什么原因导致tC2TDELAY 和 tT2CDELAY 总是为0 ?
谢谢
Yin,
请问SPIDAT1.CSHOLD是否配置为0, SPIDAT1.WDEL是否配置为1?
你好:
CSHOLD = 0;
SPIFMTn. timer_disable = 0; //18 bit of SPI Data Format Registers
SPIDAT1.WDEL 这个参数我没有配置,有关系嘛?
谢谢
Yin,
有关系,请参考spi user guide里面下面的内容:
WDEL Enable the delay counter at the end of the current transaction.
Note: The WDEL bit is supported in master mode only. In slave mode, this bit will be ignored.
0 No delay will be inserted. However, SPIx_SCS[1:0] pins will still be de-activated for at least for two
SPI peripheral clock cycles if CSHOLD = 0.
Note: In SPI, the duration for which the SPIx_SCS[1:0] pins remaining de-activated will also
depend upon time taken to supply a new data after completing the shifting operation. If the internal
buffer TXBUF is already full, then the SPIx_SCS[1:0] pins will be de-asserted for at least two SPI
peripheral clock cycles (if WDEL = 0).
1 After a transaction, WDELAY of the corresponding data format will be loaded into the delay
counter. No transaction will be performed until the WDELAY counter overflows. The SPIx_SCS
pins will be de-activated for at least (WDELAY + 2) SPI peripheral clock_Period duration.