This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 SPI2的setup time和hold time总是为0



你好:

   我们现在在DM36X平台的IPNC3.1内核下测试SPI,发现在davinci_spi_master.c中配置

iowrite32(0 | (8 << 24) | (08  << 16), davinci_spi->base + SPIDELAY);  编译后,用示波器测量clk, cs信号线,发现 tC2TDELAY 和 tT2CDELAY 总是为0, 理论上应该如图1,图2的波形才对

 图1

 图2

   请问是什么原因导致tC2TDELAY 和 tT2CDELAY 总是为0 ?

谢谢

  • Yin,

    请问SPIDAT1.CSHOLD是否配置为0, SPIDAT1.WDEL是否配置为1?

  • 你好:

       CSHOLD = 0;

      SPIFMTn. timer_disable = 0; //18 bit of SPI Data Format Registers

       SPIDAT1.WDEL 这个参数我没有配置,有关系嘛?

    谢谢

     

  • Yin,

    有关系,请参考spi user guide里面下面的内容:

    WDEL        Enable the delay counter at the end of the current transaction.
                       Note: The WDEL bit is supported in master mode only. In slave mode, this bit will be ignored.

    0      No delay will be inserted. However, SPIx_SCS[1:0] pins will still be de-activated for at least for two
    SPI peripheral clock cycles if CSHOLD = 0.
    Note: In SPI, the duration for which the SPIx_SCS[1:0] pins remaining de-activated will also
    depend upon time taken to supply a new data after completing the shifting operation. If the internal
    buffer TXBUF is already full, then the SPIx_SCS[1:0] pins will be de-asserted for at least two SPI
    peripheral clock cycles (if WDEL = 0).


    1       After a transaction, WDELAY of the corresponding data format will be loaded into the delay
    counter. No transaction will be performed until the WDELAY counter overflows. The SPIx_SCS
    pins will be de-activated for at least (WDELAY + 2) SPI peripheral clock_Period duration.

  • OK, 你说的是对的  :)

    谢谢