用的AM3354核心板做的项目,核心板是飞凌公司做的。在他们的底板上没什么问题。我自己做了一块底板,装上核心板后,按键启动有时候需要按2次才能启动,有时候1次启动,还有时候上电启动不了。另外通过串口进行系统软启动的时候也不行。
软启动:
ok335x login: root
root@ok335x:~# reboot
INIT: Sending processeStopping telnet daemon.hu Jan 15 11:35:12 20ihe system is goi
Stopping system message bus: Stopping micro-pmu...kill: usage: kill [-s sigspec | -n signum | -sigspec] pid | jobspec ... or kill -l [sigspec]
Error: Module pmudev64k is not cur
.
Stopping syslogd/klogd: stopped syslogd (pid 937)
stopped klogd (pid 938)
done
Stopping thttpd.
ALSA: Storing mixer settings...
/usr/sbin/alsactl: save_state:1580: No soundcards found...
Deconfiguring network interfaces... done.
Sending all processes the TERM signal...
Sending all processes the KILL signal...
Unmounting remote filesystems...
Deactivating swap...
Unmounting local filesystems...
Rebooting... [ 32.418067] Restarting system.
CCCCCCCC
然后就不走了。按键复位启动,有时候也会遇到。不知道什么原因。
另外我做的底板上没有将JTAG电路及接口做在上面,会不会是JTAG电路的原因呢?
望大神指教。