This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问哪里可以找到SWOSD部分的源码



专家您好:

   我使用的是dm368平台,在做OSD部分的时候发现sw_osd.h中

#define SWOSD_MAXNUMHANL 3

#define SWOSD_NUMSTREAMS 3

请问我从哪里可以找到alg_osd_ti.a的源码从而消除这个限制呢?我想实现4个通道的OSD。现在如果我创建大于3个OSD的handle就会出现异常。

另外如果无法获取此部分的源码的话,dm368的硬件OSD是如何实现的呢?我看了一些资料,但是没有找到合适的解决办法,希望您能给简单描述一下实现流程,是否需要设置启动参数,是否需要额外的接口实现叠加的OSD的数据转换等等。

谢谢!