Part Number: AM625
I referred to the device tree and defconfig specified in the linked document and enabled the LVDS backlight. However, on the LVDS screen, there was no display at all.
3.1.2.9. U-Boot Splash Screen — Processor SDK AM62x Documentation
device tree:
=> ls mmc 1
EFI/
25676288 Image
279913 tiboot3-am62x-gp-evm.bin
282502 tiboot3-am62x-hs-evm.bin
279913 tiboot3.bin
12285 ti_logo_414x97_32bpp.bmp.gz
1336827 tispl.bin
1412403 u-boot.img
574 uEnv.txt
System Volume Information/
8 file(s), 2 dir(s)
=> fatload mmc 1 $loadaddr ti_logo_414x97_32bpp.bmp.gz
12285 bytes read in 2 ms (5.9 MiB/s)
=> bmp display $loadaddr m m
=> bmp info
Image size : 414 x 97
Bits per pixel: 32
Compression : 3
I would like to know how to troubleshoot the problem. How can I make the Uboot display the logo properly? If any information is needed from me, please let me know. Thank you.