This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VEN-Q1: TDA4VEN-Q1: J722S, c7x may get stuck writing MRR registers during IPC initialization.

Part Number: TDA4VEN-Q1

Could you explain the root cause?
https://e2echina.ti.com/support/processors/f/processors-forum/1051320/tda4ven-q1-j722s-c7x-may-get-stuck-writing-mrr-registers-during-ipc-initialization

1.If I mask the mbox_fifo_write function in the omap_mbox_chan_send function, it will not be repeated (300 self-tests).
2.I speculate that it is related to the IPC message sent by the Soc core (A72/A53) to the C7X
3.When reading the MAILBOX_MAILBOX_CLUSTER_X register, I found that there was always a message in the mailbox. The interrupt trigger of the mailbox is level trigger, so it is speculated that the mailbox interrupt will continuously trigger the c7x interrupt, so I used it in several places when c7x initializes the clec register
volatile int i= 0; 
while(i<=3000000){i++;}
The c7x is busy waiting for interrupts from the soc and and finds that they are not stuck.