TMS320F28379D: 使用DMA传输spi的数据到ramgs0区域的rdata数组中,进入DMA中断查看rdata数组元素均为0,但是在中断中查询SPIRXBUFF内的数据并不为0

Part Number: TMS320F28379D

main.c内容如下:

//
// Included Files
//
#include "driverlib.h"
#include "device.h"
#include "board.h"
#include "ringpool.h"
#define  SPI_disableRXFIFO(base)   HWREGH(base + SPI_O_FFRX) &= ~SPI_FFRX_RXFIFORESET
#define  SPI_enableRXFIFO(base)     HWREGH(base + SPI_O_FFRX) |= SPI_FFRX_RXFIFORESET

__interrupt void INT_mySPI0_RX_DMA_ISR(void);



#define SPI_FRAME_LEN 21
#define PAYLOAD_LEN SPI_FRAME_LEN - 1
#pragma DATA_SECTION(rData, "ramgs0");
uint16_t rData[20];
const void *rdata = (void*)rData;
typedef enum
{
    SPI_ERR_NONE = 0,
    SPI_ERR_TIMEOUT,
    SPI_ERR_OVERRUN,
    SPI_ERR_CRC,
    SPI_ERR_DMA,
    SPI_ERR_FRAME,
} spi_error_t;


typedef enum
{
    SPI_STATE_IDLE = 0,      // 空闲
    SPI_STATE_BUSY_TX,       // 正在发送
    SPI_STATE_BUSY_RX,       // 正在接收
    SPI_STATE_BUSY_TXRX,     // 收发同时进行
    SPI_STATE_ERROR          // 错误状态
} spi_state_t;

typedef enum {
    SPI_RX_FIND_HEAD1,
    SPI_RX_FIND_HEAD2,
    SPI_RX_PAYLOAD
} spi_rx_state_t;

typedef struct
{
    volatile spi_state_t state;     // 当前状态
    volatile spi_error_t error;     // 最近一次错误

    uint16_t *tx_buf;                // 发送缓冲区
    ringpool_buffer_str rx_buf;                // 接收环形缓冲区

    uint16_t tx_len;                // 发送总长度
    uint16_t rx_len;                // 接收总长度

    uint16_t tx_cnt;        // 已发送字节数
    uint16_t rx_cnt;        // 已接收字节数

    uint32_t start_tick;             // 通信开始时间(用于超时)
    uint32_t timeout_ms;             // 超时时间

    uint16_t cs_active;               // CS 是否已拉低
} spi_comm_t;

spi_comm_t spib_com;
static spi_rx_state_t rx_state = SPI_RX_FIND_HEAD1;
//
// Main
//
void main(void)
{

    //
    // Initialize device clock and peripherals
    //
    Device_init();

    //
    // Disable pin locks and enable internal pullups.
    //
    Device_initGPIO();

    //
    // Initialize PIE and clear PIE registers. Disables CPU interrupts.
    //
    Interrupt_initModule();

    //
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    //
    Interrupt_initVectorTable();

    //
    // Board initialization
    //
    Board_init();

    ringpool_init(&spib_com.rx_buf, rData,SPI_FRAME_LEN);
    spib_com.state = SPI_STATE_IDLE;
    spib_com.tx_len = SPI_FRAME_LEN;
    spib_com.rx_len = SPI_FRAME_LEN;
    spib_com.rx_cnt = 0;
    spib_com.tx_cnt = 0;


    //
    // Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
    //
    EINT;
    ERTM;

    //
    // Loop forever. Suspend or place breakpoints to observe the buffers.
    //
    while(1)
    {
        DEVICE_DELAY_US(1000);

    }
}

__interrupt void INT_mySPI0_RX_DMA_ISR(void)
{

    // DMA_clearInterruptStatus(mySPI0_RX_DMA_BASE);

    Interrupt_clearACKGroup(INT_mySPI0_RX_DMA_INTERRUPT_ACK_GROUP);
    // uint16_t raw = SPI_readDataNonBlocking(mySPI0_BASE);
    uint16_t vaild_data = ((uint16_t*)rdata)[0];
    vaild_data = ((uint16_t*)rdata)[1];
}

board.c中各项配置如下

/*
 * Copyright (c) 2020 Texas Instruments Incorporated - http://www.ti.com
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 *
 */

#include "board.h"

//*****************************************************************************
//
// Board Configurations
// Initializes the rest of the modules. 
// Call this function in your application if you wish to do all module 
// initialization.
// If you wish to not use some of the initializations, instead of the 
// Board_init use the individual Module_inits
//
//*****************************************************************************
void Board_init()
{
	EALLOW;

	PinMux_init();
	DMA_init();
	SPI_init();
	INTERRUPT_init();

	EDIS;
}

//*****************************************************************************
//
// PINMUX Configurations
//
//*****************************************************************************
void PinMux_init()
{
	//
	// PinMux for modules assigned to CPU1
	//
	
	//
	// SPIB -> mySPI0 Pinmux
	//
	GPIO_setPinConfig(mySPI0_SPIPICO_PIN_CONFIG);
	GPIO_setPadConfig(mySPI0_SPIPICO_GPIO, GPIO_PIN_TYPE_STD);
	GPIO_setQualificationMode(mySPI0_SPIPICO_GPIO, GPIO_QUAL_ASYNC);

	GPIO_setPinConfig(mySPI0_SPIPOCI_PIN_CONFIG);
	GPIO_setPadConfig(mySPI0_SPIPOCI_GPIO, GPIO_PIN_TYPE_STD);
	GPIO_setQualificationMode(mySPI0_SPIPOCI_GPIO, GPIO_QUAL_ASYNC);

	GPIO_setPinConfig(mySPI0_SPICLK_PIN_CONFIG);
	GPIO_setPadConfig(mySPI0_SPICLK_GPIO, GPIO_PIN_TYPE_STD);
	GPIO_setQualificationMode(mySPI0_SPICLK_GPIO, GPIO_QUAL_ASYNC);

	GPIO_setPinConfig(mySPI0_SPIPTE_PIN_CONFIG);
	GPIO_setPadConfig(mySPI0_SPIPTE_GPIO, GPIO_PIN_TYPE_STD);
	GPIO_setQualificationMode(mySPI0_SPIPTE_GPIO, GPIO_QUAL_ASYNC);


}

//*****************************************************************************
//
// DMA Configurations
//
//*****************************************************************************
void DMA_init(){
    DMA_initController();
	mySPI0_RX_DMA_init();
}

void mySPI0_RX_DMA_init(){
    DMA_setEmulationMode(DMA_EMULATION_FREE_RUN);
    DMA_configAddresses(mySPI0_RX_DMA_BASE, rdata, mySPI0_RX_DMA_ADDRESS);
    DMA_configBurst(mySPI0_RX_DMA_BASE, 1U, 0, 0);
    DMA_configTransfer(mySPI0_RX_DMA_BASE, 20U, 1, 1);
    DMA_configWrap(mySPI0_RX_DMA_BASE, 20U, 0, 20U, 0);
    DMA_configMode(mySPI0_RX_DMA_BASE, mySPI0_RX_DMA_TRIGGER, DMA_CFG_ONESHOT_DISABLE | DMA_CFG_CONTINUOUS_ENABLE | DMA_CFG_SIZE_16BIT);
    DMA_setInterruptMode(mySPI0_RX_DMA_BASE, DMA_INT_AT_END);
    DMA_enableInterrupt(mySPI0_RX_DMA_BASE);
    DMA_disableOverrunInterrupt(mySPI0_RX_DMA_BASE);
    DMA_enableTrigger(mySPI0_RX_DMA_BASE);
    DMA_startChannel(mySPI0_RX_DMA_BASE);
}

//*****************************************************************************
//
// INTERRUPT Configurations
//
//*****************************************************************************
void INTERRUPT_init(){
	
	// Interrupt Settings for INT_mySPI0_RX_DMA
	// ISR need to be defined for the registered interrupts
	Interrupt_register(INT_mySPI0_RX_DMA, &INT_mySPI0_RX_DMA_ISR);
	Interrupt_enable(INT_mySPI0_RX_DMA);
}
//*****************************************************************************
//
// SPI Configurations
//
//*****************************************************************************
void SPI_init(){
	mySPI0_init();
}

void mySPI0_init(){
	SPI_disableModule(mySPI0_BASE);
	SPI_setConfig(mySPI0_BASE, DEVICE_LSPCLK_FREQ, SPI_PROT_POL1PHA0,
				  SPI_MODE_PERIPHERAL, mySPI0_BITRATE, mySPI0_DATAWIDTH);
	SPI_setPTESignalPolarity(mySPI0_BASE, SPI_PTE_ACTIVE_LOW);
	SPI_enableFIFO(mySPI0_BASE);
	SPI_setFIFOInterruptLevel(mySPI0_BASE, SPI_FIFO_TXEMPTY, SPI_FIFO_RX1);
	SPI_clearInterruptStatus(mySPI0_BASE, SPI_INT_RXFF);
	SPI_enableInterrupt(mySPI0_BASE, SPI_INT_RXFF);
	SPI_disableLoopback(mySPI0_BASE);
	SPI_setEmulationMode(mySPI0_BASE, SPI_EMULATION_STOP_AFTER_TRANSMIT);
	SPI_enableModule(mySPI0_BASE);
}

  • 您好,
    已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • 您好,

         请检查配置和代码,确保它遵循这里列出的步骤和设置:

         

    是否也能确保已将 DMA 配置为secondary master of peripheral frame 2(包含 SPI 寄存器总线)?

    可以在初始化之后添加以下代码行来实现这一点。请参阅此处 TRM 中的相关部分。没有此配置,DMA 对 SPI 寄存器的写入将不会生效。

     SysCtl_selectSecController(SYSCTL_SEC_CONTROLLER_DMA, SYSCTL_SEC_CONTROLLER_DMA);

  • 谢谢您的回复,在初始化部分添加了

     SysCtl_selectSecController(SYSCTL_SEC_CONTROLLER_DMA, SYSCTL_SEC_CONTROLLER_DMA);
    后可以进入DMA中断且接收缓存区有数值,但是我遇到了新的问题,接收缓存区的数据存在一部分无效数据,如下图所示

    在SPI通信中ARM芯片作为主机,DSP作为从机,请问遇到此种情况一般是哪些问题导致的,当我不使用DMA,单纯的轮询接收与发送时,可以正常的接收SPI通信报文

  • 您好,

         如能够让轮询方式正常工作,这似乎是DMA设置的问题。

        我看到DMA配置代码有一些问题,您是通过在SPI系统配置中添加接收DMA子模块生成的代码吗?还是DMA是手动添加的?

  • 我在SPI系统配置中添加接收DMA子模块生成的代码(syscfg生成),请问是哪里存在问题

    我移除DMA外设后,只用SPI中断接收数据发现了同样的问题,这是我的中断接收代码:

    SPI中断接收:

    void SPI_init(){
    mySPI0_init();
    }

    void mySPI0_init(){
    SPI_disableModule(mySPI0_BASE);
    SPI_setConfig(mySPI0_BASE, DEVICE_LSPCLK_FREQ, SPI_PROT_POL1PHA0,
    SPI_MODE_PERIPHERAL, mySPI0_BITRATE, mySPI0_DATAWIDTH);
    SPI_setPTESignalPolarity(mySPI0_BASE, SPI_PTE_ACTIVE_LOW);
    SPI_enableFIFO(mySPI0_BASE);
    SPI_setFIFOInterruptLevel(mySPI0_BASE, SPI_FIFO_TXEMPTY, SPI_FIFO_RX1);
    SPI_clearInterruptStatus(mySPI0_BASE, SPI_INT_RXFF);
    SPI_enableInterrupt(mySPI0_BASE, SPI_INT_RXFF);
    SPI_disableLoopback(mySPI0_BASE);
    SPI_setEmulationMode(mySPI0_BASE, SPI_EMULATION_STOP_AFTER_TRANSMIT);
    SPI_enableModule(mySPI0_BASE);
    }

    void main(void)
    {

    //
    // Initialize device clock and peripherals
    //
    Device_init();

    //
    // Disable pin locks and enable internal pullups.
    //
    Device_initGPIO();

    //
    // Initialize PIE and clear PIE registers. Disables CPU interrupts.
    //
    Interrupt_initModule();

    //
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    //
    Interrupt_initVectorTable();

    //
    // Board initialization
    //
    Board_init();
    // DMA_stopChannel(mySPI0_RX_DMA_BASE);

    // SysCtl_selectSecController(SYSCTL_SEC_CONTROLLER_DMA, SYSCTL_SEC_CONTROLLER_DMA);


    ringpool_init(&spib_com.rx_buf, rData,SPI_FRAME_LEN);
    spib_com.state = SPI_STATE_IDLE;
    spib_com.tx_len = SPI_FRAME_LEN;
    spib_com.rx_len = SPI_FRAME_LEN;
    spib_com.rx_cnt = 0;
    spib_com.tx_cnt = 0;


    //
    // Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
    //
    EINT;
    ERTM;

    //
    // Loop forever. Suspend or place breakpoints to observe the buffers.
    //
    while(1)
    {
    DEVICE_DELAY_US(1000);
    }
    }

    __interrupt void INT_mySPI0_RX_ISR(void)
    {
    while (SPI_getRxFIFOStatus(mySPI0_BASE) > 0)
    {
    uint16_t data = SPI_readDataNonBlocking(mySPI0_BASE);

    // 立刻预装下一个字节
    if (SPI_getTxFIFOStatus(mySPI0_BASE) != SPI_FIFO_TXFULL)
    {
    SPI_writeDataNonBlocking(mySPI0_BASE, 0xFF);
    }
    }

    SPI_clearInterruptStatus(mySPI0_BASE, SPI_INT_RXFF);
    Interrupt_clearACKGroup(INT_mySPI0_RX_INTERRUPT_ACK_GROUP);
    }

  • 您好,

         请评估下面建议:

    • 指向 rData 缓冲区的指针和缓冲区本身使用不同的名称。编译器可能会认为它们是同一件事,因为它们具有相同的符号。请试一下:
      • const void *rdataPtr = (void*)rData;
    • DMA destination burst step请使用 1,这样每个值就不会写入缓冲区的同一个位置
      • DMA_configBurst(mySPI0_RX_DMA_BASE, 1U, 0, 1);
    • DMA source transfer step请使用 0,因为只需要源地址保持在 SPI 接收缓冲区地址
      • DMA_configTransfer(mySPI0_RX_DMA_BASE, 20U, 0 1);
    • 不建议在这里使用 wrap 功能,在每次新的传输开始时,如果想做的是将源和目标指针重置回原始值,它们已经会被重置。只有当想改变每次传输的起始位置时,才应该使用 wrap。如果始终只是将数据从 SPI RX 缓冲区移动到 rData 数组中,可以保持每次的起始地址不变(源为 SPI RX 缓冲区的地址,目标为 rData 数组的起始位置)。
      • DMA_configWrap(mySPI0_RX_DMA_BASE, 65535U, 0, 65535U, 0);