This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好 :
這是我第一次使用DSP,我採用的板子是EVMK2H
照user guide 安裝後,
MCSDK的版本3_01_04_07
CCS的版本為v5
我利用CCS跑hello.c
下面是我的target configuration
其中我的 C66XX_0的GEL為 mcsdk_bios_3_01_04_07\tools\program_evm\gel\xtcievmk2x.gel
這是我的console的結果
C66xx_0: GEL Output:
Connecting Target...
C66xx_0: GEL Output: TCI6638K2K GEL file Ver is 1.3
C66xx_0: GEL Output: Detected PLL bypass disabled: SECCTL[BYPASS] = 0x00000000
C66xx_0: GEL Output: (3a) PLLCTL = 0x00000040
C66xx_0: GEL Output: (3b) PLLCTL = 0x00000040
C66xx_0: GEL Output: (3c) Delay...
C66xx_0: GEL Output: (4)PLLM[PLLM] = 0x0000000F
C66xx_0: GEL Output: MAINPLLCTL0 = 0x07000000
C66xx_0: GEL Output: (5) MAINPLLCTL0 = 0x07000000
C66xx_0: GEL Output: (5) MAINPLLCTL1 = 0x00000040
C66xx_0: GEL Output: (6) MAINPLLCTL0 = 0x07000000
C66xx_0: GEL Output: (7) SECCTL = 0x00090000
C66xx_0: GEL Output: (8a) Delay...
C66xx_0: GEL Output: PLL1_DIV3 = 0x00008002
C66xx_0: GEL Output: PLL1_DIV4 = 0x00008004
C66xx_0: GEL Output: PLL1_DIV7 = 0x00000000
C66xx_0: GEL Output: (8d/e) Delay...
C66xx_0: GEL Output: (10) Delay...
C66xx_0: GEL Output: (12) Delay...
C66xx_0: GEL Output: (13) SECCTL = 0x00090000
C66xx_0: GEL Output: (Delay...
C66xx_0: GEL Output: (Delay...
C66xx_0: GEL Output: (14) PLLCTL = 0x00000041
C66xx_0: GEL Output: PLL has been configured (CLKIN * PLLM / PLLD / PLLOD = PLLOUT):
C66xx_0: GEL Output: PLL has been configured (122.88 MHz * 16 / 1 / 2 = 983.04 MHz)
C66xx_0: GEL Output: Power on all PSC modules and DSP domains...
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=2, md=9!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=17, md=25!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=17, md=26!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=18, md=27!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=19, md=28!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=19, md=29!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=20, md=30!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=20, md=31!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=20, md=32!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=20, md=33!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=21, md=34!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=22, md=35!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=22, md=36!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=23, md=37!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=23, md=38!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=24, md=39!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=24, md=40!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=24, md=41!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=24, md=42!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=25, md=43!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=25, md=44!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=25, md=45!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=25, md=46!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=26, md=47!
C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=27, md=48!
C66xx_0: GEL Output: Power on all PSC modules and DSP domains... Done.
C66xx_0: GEL Output: WARNING: SYSCLK is the input to the PA PLL.
C66xx_0: GEL Output: Completed PA PLL Setup
C66xx_0: GEL Output: PAPLLCTL0 - before: 0x0x07080400 after: 0x0x07080400
C66xx_0: GEL Output: PAPLLCTL1 - before: 0x0x00002040 after: 0x0x00002040
C66xx_0: GEL Output: DDR begin
C66xx_0: GEL Output: XMC setup complete.
C66xx_0: GEL Output: DDR3 PLL (PLL2) Setup ...
C66xx_0: GEL Output: DDR3 PLL Setup complete, DDR3A clock now running at 666 MHz.
C66xx_0: GEL Output: DDR3A initialization complete
C66xx_0: GEL Output: DDR3 PLL Setup ...
C66xx_0: GEL Output: DDR3 PLL Setup complete, DDR3B clock now running at 800MHz.
C66xx_0: GEL Output: DDR3B initialization complete
C66xx_0: GEL Output: DDR done
C66xx_0: Trouble Writing Memory Block at 0xa020 on Page 0 of Length 0x13e: (Error -1190 @ 0x20) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.232.0)
C66xx_0: GEL: File: C:\Users\Lab333\workspace_v5_5\abcde\Debug\abcde.out: Load failed.
目前一直卡在這裡,重新安裝數次以及更新版本,問題仍未解決
可以告訴我說 這問題可能是哪裡出錯嗎? 謝謝!
你换一个gel文件试试看,我一般使用的是CCS安装目录下的gel
C:\CCS_6_1_1\ccsv6\ccs_base\emulation\boards\xtcievmk2x\gel
您好,我有換過gel的檔案 並且也更新到CCS_6_1 但還是有一樣問題
謝謝!
也有可能是仿真器连接的问题,你运行一下ccxml文件的test connection文件,看看仿真器能否正常连接上EVM。
您好 我現在使用的gel的路徑為 ../../../../mcsdk_bios_3_01_04_07/tools/program_evm/gel/xtcievmk2x.gel
下面為test connection的結果
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
/home/lab329/.TI/1298036012/0/0/BrdDat/testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
The library build date was 'Aug 20 2013'.
The library build time was '23:33:52'.
The library package version is '5.1.232.0'.
The library component version is '35.34.40.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '12' (0x0000000c).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
This emulator does not create a reset log-file.
-----[Perform the Integrity scan-test on the JTAG IR]------------------------
This test will use blocks of 512 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG IR Integrity scan-test has succeeded.
-----[Perform the Integrity scan-test on the JTAG DR]------------------------
This test will use blocks of 512 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG DR Integrity scan-test has succeeded.
[End]
以下為目前console的結果
謝謝你的協助!