This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3530 GPMC 配置不对

Other Parts Discussed in Thread: OMAP3530

小弟最近在linux下做一个驱动,OMAP3530通过GPMC与FPGA进行通信,速度要求为大于20.48MByte,我想通过异步的方式进行传输。通过配置,从ARM端得到了一个稳定的时序如图:




我的配置如下:
#define FPGA_GPMC_CONFIG1 0x00001000
#define FPGA_GPMC_CONFIG2 0x000a0a00                //CSRDACCESSTIME=10,   CSWRACCESSTIME=10
#define FPGA_GPMC_CONFIG3 0x00020200                   //ADVRDOFFTIME=2,     ADVWROFFTIME=2
#define FPGA_GPMC_CONFIG4 0x08050805                   //OEOFFTIME=8,   WEOFFTIME=8,   OEONTIME=5,   WEONTIME=5
#define FPGA_GPMC_CONFIG5 0x00080b0b                //RDCYCLETIME=11,    WRCYCLETIME=11
#define FPGA_GPMC_CONFIG6 0x08000000                   //WRACCESSTIME=8

我的问题如下,如图,我设置的是两次连续读取之间的时间间隔为0,得到的时序中可以看到,两次CS拉低之间有很长一段高电平,占用了大量的时间,远远达不到20M的要求。一时间找不到原因。