This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!我现在你使用的是OMAP3530平台,DSP是3730。想了解下手册中的SWE和SWENR指令是什么?它们有什么用途?如何使用?
TI是否有相关的文档介绍?
OMAP3530是C64+的DSP核,参考文档spru732j:
SWE:
Description Causes an internal exception to be taken. It can be used as a mechanism for User mode
programs to request Supervisor mode services. Execution of the SWE instruction results
in an exception being recognized in the E1 pipeline phase containing the SWE
instruction. The SXF bit in EFR is set to 1. The HWE bit in NTSR is cleared to 0. If
exceptions have been globally enabled, this causes an exception to be recognized
before execution of the next execute packet. The address of that next execute packet is
placed in NRP.
SWENR:
Description Causes an internal exception to be taken. It is intended for use in systems supporting a
secure operating mode. It can be used as a mechanism for User mode programs to
request Supervisor mode services. It differs from the SWE instruction in four ways:
1. TSR is not copied into NTSR.
2. No return address is placed in NRP (it remains unmodified).
3. The IB bit in TSR is set to 1. This will be observable only in the case where another
exception is recognized simultaneously.
4. A branch to REP (restricted entry point register) is forced in the context switch rather
than the ISTP-based exception (NMI) vector.
This instruction executes unconditionally.
If another exception (internal or external) is recognized simultaneously with the
SWENR-raised exception then the other exception(s) takes priority and normal exception
behavior occurs; that is, NTSR and NRP are used and execution is directed to the NMI
vector.