This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dvs8148 Hdvpss DVO2输出



您好:

      我现在想通过hdvpss的Aux Input Path作为显示的输入通路,通过DVO2将视频数据传递给sii9134芯片。

     我使用的软件版本为ipnc3.8.DEMO是multich_capturedisplay.c。

      我在multich_capturedisplay.c中设定了

             capturePrm.outQueParams[0].nextLink = gVdisModeleContext.dispalyId[VDIS_DEV_DVO2];

             displayPrm.displayId= Display_LINK_DISPLAY_SC2.

        要求视频输出格式是视频数据与同步信号分离的模式。

      目前的现象是8148测不到输出的视频数据。通过打印得知显示控制的设置为:Aux-->vcomp_pip_select->vcomp.

    问题1: 我想知道这样的路径是不是有问题,我认为应该是AUX-->DVO2_SELECT,如果按照Aux-->vcomp_pip_select->vcomp.这种设置,我要通过                 设置那个寄存器使得视频数据从的dvo2输出呢?

    问题2:HDVPSS Detailed Block Diagram中CIG模块可以接收Primary以及Aux的数据,是如何选择的,CIG模块中的(cf)是什么意思?