This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在dm8127平台下,IR_CUT反复切换



您好!

  在dm8127平台下IR_CUT问题,IR_CUT有时候在光线较暗的情况下一直不停的来回切换。

在dm8127芯片上好像有对IR_CUT切换的控制,如下图:

图中CDS(AF27)和IREN(AE26)好像可以对IR_CUT进行控制,项目中使用了一个光敏二极管来控制IR_CUT的切换,CDS 直接与光敏二极管相连,测量出CDS显示的是电压值,当CDS上的电压值为2V时,IR_CUT刚好切换。

请问,dm8127 RDK中有对IR_CUT的控制吗?我现在想要通过软件来对IR_CUT切换进行控制,请问怎样做?还有IR_CUT光线较弱时反复切换是什么原因造成的?

  • Wei Zhimin,

    请问你使用的是Appro的2A么?Appro的2A算法里面有对IR filter控制的相关代码,但Appro的2A提供的是库。

    你看看下面的论坛讨论是否对你有所帮助?

    https://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/p/420838/1562761#pi317334=2

  • 您好,感谢您的回答

       后来我仔细看了测量下,我们做的板子上有IDS和IREN脚,可以读出电压的变化和高低电平的,但是dm8127芯片上没有ADC所以没办法通过软件来读出电压值。只能通过更改硬件来控制IR_CUT的切换。问题通过更改硬件已解决,再次感谢你。