This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678如何发挥GbE千兆以太网的性能达到500Mbps?



最近在调试DSP6678千兆以太网通信,希望实现500Mbps的通信速率;

采用两种方法进行了测试,结果发现通信速率都不高:

1. 采用NDK UDP发送,软件架构是开辟一个UDP_send任务线程while(1)循环sendto发送1024个字节到PC:

	while(1)
	{
		nLen = 0;

		I = sendto(sudp, (char *)dataNet, PACK_LEN, 0, (PSA)&sin1, m_nAddrLen);
		TaskSleep(1);
		//TaskSleep(1);
		//asm(" NOP 5");
//		uCounter = 0;
//		while(uCounter<100000000)
//		{
//			uCounter++;
//		}
	}

为了调节发送速度,修改TaskSleep()的时间,最小设置为1,在PC端显示的接受速度为几十Mbps,然而改用自己设置的延时,发现根本就发送不出去,有些时候即使是使用TaskSleep(1),有些时候好像也会出现数据发送不出去的现象。

我想问一下,为何只能使用TaskSleep进行延时,而且延时时间短了,还会出现发送不出去的现象?

那么NDK发送数据到PC,最快的速度能到多少Mbps?

2. 使用PAexample中的配置如下:

Int32 SendPacket (Void)
{
    Cppi_Desc*      pCppiDesc;
    UInt32          dataBufferSize;
    char            psFlags = (cpswSimTest)?pa_EMAC_PORT_0:pa_EMAC_PORT_1; /* pa_EMAC_PORT_1上挂的有RJ45 */

    /* Get a free descriptor from the global free queue we setup 
     * during initialization.
     */
    if ((pCppiDesc = Qmss_queuePop (gTxFreeQHnd)) == NULL) /* 从发送free queues中pop出一个descriptors出来 */
    {
        System_printf ("No Tx free descriptor. Cant run send/rcv test \n");
        return -1;
    }

    /* The descriptor address returned from the hardware has the 
     * descriptor size appended to the address in the last 4 bits.
     *
     * To get the true descriptor size, always mask off the last 
     * 4 bits of the address.
     */
    pCppiDesc = (Ptr) ((UInt32) pCppiDesc & 0xFFFFFFF0);    

    dataBufferSize  =   sizeof (pktMatch);

    /* 给 descriptors 设置数据,也就是要发送的数据pktMatch,UDP数据源包 */
    Cppi_setData (  Cppi_DescType_HOST, 
                    (Cppi_Desc *) pCppiDesc, 
                    (UInt8 *) Convert_CoreLocal2GlobalAddr((UInt32)pktMatch), 
                    dataBufferSize
                 );
    /* 设置packet length */
    Cppi_setPacketLen (Cppi_DescType_HOST, (Cppi_Desc *)pCppiDesc, dataBufferSize);
    
    if (cpswLpbkMode != CPSW_LOOPBACK_NONE)
    {
        /* Force the packet to the specific EMAC port if loopback is enabled */
        Cppi_setPSFlags(Cppi_DescType_HOST, (Cppi_Desc *)pCppiDesc, psFlags);
    }
    else
    {
        /* 这样去设置PS flags */
    	Cppi_setPSFlags(Cppi_DescType_HOST, (Cppi_Desc *)pCppiDesc, 0);
    }
  
    /* Send the packet out the mac. It will loop back to PA if the mac/switch 
     * have been configured properly 
     */  
    /* 将这个描述符descriptor压入到PA的Tx queue中,这里选择的是queue 648 SwTx0, 送入到队列尾部 */
    Qmss_queuePush (gPaTxQHnd[8], pCppiDesc, dataBufferSize, SIZE_HOST_DESC, Qmss_Location_TAIL);

    /* Increment the application transmit counter */
    gTxCounter ++;

    /* Give some time for the PA to process the packet */
    CycleDelay (200000); // 1ms

    // 试试能不能回收
    Qmss_queuePush (gTxFreeQHnd, pCppiDesc, dataBufferSize, SIZE_HOST_DESC, Qmss_Location_TAIL);


    return 0; 
}

这里面发送最后也要进行延时等待,等待PA处理完毕,我想知道PA处理得多快?我设置延时时间稍微短一下,就出现数据没有发送出去的现象,感觉GbE千兆以太网只有百兆以太网的效果,根本达不到我想要实现的高速接口的作用。

想问一下,TI有没有相关的测试文档说明GbE究竟能够实现多少通信速率?