专家们好,PCIe评估板上PCIe部分原理图让我比较疑惑,在12页的PCIe部分0.1uf的耦合电容放置到了Rx一端,这个和PCIe规范是不一致的,在PCI Express Base Specification,Revision 2.1中4.3.5.1中提到 “Capacitors must be placed on the Transmitter side of an interface that permits adapters to be plugged and unplugged.....”,也就是说,如果要进行板级互联,耦合电容应该放置到发送端,我查看了一些其他PCIe板卡,他们的耦合电容全部放在了发送端,但6678评估板上放置到了接收端,不知道是不是有什么考虑?希望专家解答 。谢谢