This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教专家PCIe 耦合电容放置位置问题!



专家们好,PCIe评估板上PCIe部分原理图让我比较疑惑,在12页的PCIe部分0.1uf的耦合电容放置到了Rx一端,这个和PCIe规范是不一致的,在PCI Express Base Specification,Revision 2.1中4.3.5.1中提到 “Capacitors must be placed  on the Transmitter side of  an interface that permits adapters to be plugged and unplugged.....”,也就是说,如果要进行板级互联,耦合电容应该放置到发送端,我查看了一些其他PCIe板卡,他们的耦合电容全部放在了发送端,但6678评估板上放置到了接收端,不知道是不是有什么考虑?希望专家解答 。谢谢

  • 您好,

    请结合第10页amc部分的AMCC_P4_PCIe_TX1P信号处,也有0.1uF的耦合电容。说明在此6678评估板上RX和TX端都是接了耦合电容的。

    PCIe的耦合电容放在TX端的原因您已经提到了。

    至于为什么在RX端和TX端都加耦合电容,我想除了高速信号传输需要AC耦合之外,还有一个原因是:amc的工作电压在12V,而6678工作电压在1~2v,两个不同工作电压的系统相连接时,加一个耦合电容,利用电容隔值的原理可以起到保护作用。