我目前使用的是IPNC RDK3.5,我想使用VNF模块中的affine功能
我发现如果开启这个功能,单一一个channel 1080P FPS会降到23左右
(VNF其余的降噪功能或LDC都是关闭的)
计算了下affine所需要的时间,发现平均一张大概落在36~40ms
请问这个是硬件本身速度的限制吗? 还是我哪里没有配置好?
谢谢各位大神帮忙!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Lee Weiyu,
affine是基于LDC的。请问你使用的输入是YUV422还是YUV420的,不同的输入,性能上也是有区别的。
还有M3的频率目前配置的是否是芯片支持的最高频率? CYE3可以支持560MHz M3,M3的频率也会影响到LDC的性能。