This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于6472的pllc模式的选择问题



专家您好,刚开始学习6472的CSL库不久,今天有个问题困扰了我一天,想来请教你们一下:

pllc工作有两种模式:bypass模式和pll模式。在6455的csl_pllc.h中CSL_PllcHwSetup结构体定义了Uint32   pllMode这么一个变量,可以方便的进行设置,而今天我看6472的csl_pllc.h中CSL_PllcHwSetup结构体根本没有pllMode这个变量,也没有预分频的preDiv变量,这是为什么呢?如果要更改设置该怎么办?CSL文件是从官网下的,应该没有问题。

还有一个问题,关于这两个模式,bypass模式下输入信号直接就到分频器,pll模式下输入信号经过PREDIV、PLLM再到了分频器,那么是否我要用PLLM提高输入时钟的频率那就必须用PLL模式?

  • 您好,请先参考TMS320C6472 (PLL) Controller User's Guide。www.ti.com.cn/.../spru806a.pdf

  • Melody Chen您好:

    user guide我也看过,但是它也没提到关于CSL的问题,6472的CSL API REFERRENCE我也看了,也没提到这个模式的选择问题,只有一句

    #define CSL_PLLC_CTRL_BYPASS CSL_FMKT (PLLC_PLLCTL_PLLEN, BYPASS)

    #define CSL_PLLC_CTRL_ENABLE CSL_FMKT (PLLC_PLLCTL_PLLEN, PLL)

    在6455中,是这么设置的

    typedef struct CSL_PllcHwSetup {

       /** \brief PLL Mode PLL/BYPASS

         * This is valid only for PLLC instance 1

         */

       Uint32        pllMode;

    ......

    } CSL_PllcHwSetup;

    而6472的CSL中,并没有这个选项,所以我现在不知道该怎么办了