This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS5.5导入Image_processing_evmc6678l工程编译错误

Other Parts Discussed in Thread: SYSBIOS

各个前辈,你们好!

1、在CCS5.5环境下导入mcsdk_2_01_02_06下的image_processing_evmc6678l_master、image_processing_evmc6678l_slave两个工程出现错误,而mcsdk_2_01_02_06下HUA工程等都没有错误。错误详细情况在doc文档中

问题描述:

在导入image_processing_evmc6678l_master、 Image_processing_evmc6678l_slave两个工程后,进行编译出现了如下错误:

1最开始masterslave工程编译的错误是一样的:

 

而后将master的几个libinc路径更改到本地安装的路径上,同时将UIA去掉

就由上述错误转变为:

'Building file: ../image_processing_evmc6678l_master.cfg'

'Invoking: XDCtools'

"C:/ti/xdctools_3_25_03_72/xs" --xdcpath="C:/ti/ipc_1_24_03_32/packages;C:/ti/ndk_2_24_02_31/packages;C:/ti/bios_6_33_06_50/packages;C:/ti/mcsdk_2_01_02_06;C:/ti/imglib_c66x_3_1_1_0/packages;C:/ti/pdk_C6678_1_1_2_6/packages;C:/ti/mcsdk_2_01_02_06/demos;C:/ti/ccsv5/ccs_base;" xdc.tools.configuro -o configPkg -t ti.targets.elf.C66 -p demos.image_processing.ipc.evmc6678l.platform -r debug -c "C:/ti/ccsv5/tools/compiler/c6000_7.4.18" "../image_processing_evmc6678l_master.cfg"

making package.mak (because of package.bld) ...

generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...

configuring image_processing_evmc6678l_master.xe66 from package/cfg/image_processing_evmc6678l_master_pe66.cfg ...

js: "C:/ti/mcsdk_2_01_02_06/demos/image_processing/ipc/evmc6678l/master/image_processing_evmc6678l_master.cfg", line 141: xdc.services.global.XDCException: xdc.PACKAGE_NOT_FOUND: can't locate the package 'ti.uia.runtime' along the path: 'C:/ti/ipc_1_24_03_32/packages;C:/ti/ndk_2_24_02_31/packages;C:/ti/bios_6_33_06_50/packages;C:/ti/mcsdk_2_01_02_06;C:/ti/imglib_c66x_3_1_1_0/packages;C:/ti/pdk_C6678_1_1_2_6/packages;C:/ti/mcsdk_2_01_02_06/demos;C:/ti/ccsv5/ccs_base;C:/ti/xdctools_3_25_03_72/packages;..;'. Ensure that the package path is set correctly.

    "./package/cfg/image_processing_evmc6678l_master_pe66.cfg", line 188

gmake.exe: *** [package/cfg/image_processing_evmc6678l_master_pe66.xdl] Error 1

js: "C:/ti/xdctools_3_25_03_72/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.

gmake[1]: *** [configPkg/linker.cmd] Error 1

gmake[1]: Target `main-build' not remade because of errors.

gmake: *** [all] Error 2

**** Build Finished ****

2、目前使用的是CCS5.5版本,所使用的板子是C6678l评估板,有没有必要将CCS5.5升级为CCS6.1?ccs6.1软件是否更好的支持C6678 基于bios内核应用开发。

关于上述两个问题,希望请教一下各位,在下感激不敬。