This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6748 NAND FLASH问题



请问6748最大能支持多少GB的NAND FLASH?

  • 基于NAND flash的访问特性,大小没有限制。

    问题是你要用来做boot,还是只是存数据。

    做boot设备的话,跟ROM的软件支持相关。一般来说支持到2Kbyte page size。详情见文档里的支持列表:http://www.ti.com/lit/pdf/spraat2

  • 感谢回复!我是用来存数据的!呵呵!这样是不是我就可以把2GB大容量的NAND FLASH用上了?

     

  • 绝对可以。

    唯独要注意的一点是,选择NAND型号时,下面的时序要求:

    18.2.5.6.8 Interfacing to a Non-CE Don't Care NAND Flash
    As explained in Section 18.2.5.6.4, the EMIFA does not support NAND Flash devices that require the chip
    select signal to remain low during the tR time for a read. One way to work around this limitation is to use a
    GPIO pin to drive the CE signal of the NAND Flash device. If this work around is implemented, software
    will configure the selected GPIO to be low, then begin the NAND Flash operation, starting with the
    command phase. Once the NAND Flash operation has completed the software can then configure the
    selected GPIO to be high.

  • 能推荐一款芯片型号么?要求工业级!

  • 下面链接里的型号是验证成功使用的,不代表其它的不能用。可以上NAND厂家的网站上去查询更多的型号。

    http://processors.wiki.ti.com/index.php/List_of_NANDs_devices_supported_by_TI_RBLs#OMAPL138.2FC6748.2FC6746.2FC6742.2FAM18xx

  •  你好:

                我用的是OMAPL138,外挂的NANDFlash是MT29F32G08ABABA,该芯片支持ONFI 2.2版本,NAND大小4GB,Pagesize 8KB。用来存boot和文件系统,调试uboot的时候发现程序存在异常,能够正常运行的uboot,不能随意修改代码,比如增加一行或者删除一行无关的代码,boot就无法启动或者启动一半后重启。

               想知道OMAPL138 是否是不支持8KB Pagesize 的NAND启动,但是手册里面又讲了是完全支持 ONFI协议的啊!

                  谢谢!

                 坐等,急!非常感谢!