dm6467t是否支持上述压缩要求和什么设置有关系?
256*256,100fps,14位灰度值,使用H.264编码压缩。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
dm6467t是否支持上述压缩要求和什么设置有关系?
256*256,100fps,14位灰度值,使用H.264编码压缩。
Shi Gaotao,
H264标准编码输入应该是YUV420的,不是灰度。如果是8-bit灰度,你可以人工制造UV的值,但14-bi的灰度,无法保证14-bit的精度。
这样啊,那就悲剧了。是不是可以理解H264本身就不支持14bit的灰度?
Shi Gaotao,
下面的信息可以在DM6467的h264enc datasheet里面找到:
YUV420 interleaved color sub-sampling (Y as a
single plane and U and V components
interleaved to form the second plane) formats
supported
继续请教,dm6467t带的编码算法提供的API是否有传递视频帧的灰度值的参数?
谢谢。
Shi Gaotao,
H264编码输入是YUV420sp。Y是8-bit,U或者V也是8-bit,这是固定的。没有你说的这个灰度值参数。编码的参数请参考编码的user guide。