使用C6748 的SPI1传输图像,为了增速使用了EDMA3,SPI1的频率设置为最大。最后测得速度大约为0.37MByte/s.
得到的结果没有达到1MByte/s 以上。
SPI理论上的速度是可以达到1MByte/s 以上的,请问C6748 的SPI传输速度最大能达到多少?EDMA3的设置能够提速多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用C6748 的SPI1传输图像,为了增速使用了EDMA3,SPI1的频率设置为最大。最后测得速度大约为0.37MByte/s.
得到的结果没有达到1MByte/s 以上。
SPI理论上的速度是可以达到1MByte/s 以上的,请问C6748 的SPI传输速度最大能达到多少?EDMA3的设置能够提速多少?
你可以测试一下SPI FLASH的读写速度,0.37MB/S有没有可能和SPI DEVICE速度有关系?
我这边没有6748的数据,AM335X读是可以达到1M以上的,6748开EDMA应该速度差不多。
我设置C6748的SPI作为主机,从机是另外一个MCU的SPI。我测试的时候没连接从机,速度是由主机决定的。C6748的SPI只是发送数据,我连续发送65535个字节的数据,测试速度。所以速度可能和SPI DEVICE速度没有关系。
现在需要确定是我的配置不好,还是C6748在加上EDMA3之后的速度就只能达到0.3MByte左右?
“AM335X读是可以达到1M以上”是1Mbit/s还是1MByte/s?