This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6748 SPI 的最大传输速度



使用C6748 的SPI1传输图像,为了增速使用了EDMA3,SPI1的频率设置为最大。最后测得速度大约为0.37MByte/s.

得到的结果没有达到1MByte/s 以上。

SPI理论上的速度是可以达到1MByte/s 以上的,请问C6748 的SPI传输速度最大能达到多少?EDMA3的设置能够提速多少?