This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位好:
使用自己研制的硬件版做4路pal视频数据采集编码,采集芯片使用1片TVP5158,TVP5158数据出来进入到FPGA,由FPGA处理成一路8-bit bt565数据流,再由FPGa通过vportB口发送个DM8418进行处理;使用的是DVR RDK中4D1的usecase;经过示波器测试,DM8148VPORT口已经有数据输入了。
问题是:对编码后的数据进行存盘,但并没有数据可以保存。
个人认为,问题可能是采集link capture并没有收到正确格式数据,导致capture没有输出,所以编码enc也没有输出;
请问:1.DVR RDK是否有可以看到数据采集情况的程序接口?
2.由于只用了2个摄像头,所以是由FPGA将2路视频数据复制为4路,在形成8bit-bt656码流给8148,这种处理方式有没有什么问题?
感谢回答!!!
Ran Yang,
DM8148可以直接介入TVP5158的输出,并且把4路D1拆分出来,为什么你还要加一个FPGA?
你的FPGA输出1路BT656,也是和TVP5158一样的line interlaved的模式/格式吗? 不然DM8148如何解析出4路D1?
你可以看看CaptureLink_drvCallback函数是否有执行到。