误以为UPP_D3引脚(编号153)可以配置为普通GPIO使用,实际上6748只有141个GPIO,将UPP_D3,UPP_D4,SPI1_CLK作为了FPGA的配置电路,需要用这三个引脚产生一个配置时序,但UPP的数据引脚并不能当成普通GPIO使用,电路已经设计好,还有没有补救办法?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
误以为UPP_D3引脚(编号153)可以配置为普通GPIO使用,实际上6748只有141个GPIO,将UPP_D3,UPP_D4,SPI1_CLK作为了FPGA的配置电路,需要用这三个引脚产生一个配置时序,但UPP的数据引脚并不能当成普通GPIO使用,电路已经设计好,还有没有补救办法?
就是PINMUX寄存器中无法配置这个引脚为GPIO,所以不能直接控制它的输出。
VP_DIN[11] / UHPI_HD[3] / UPP_D[3] / PRU0_R30[11] / PRU0_R31[11] R18
是这个脚吗?的确没办法配成GPIO
目前看来最简单的方法,想法飞跟GPIO的线过来吧。