This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 power-on Sequence 问题

Other Parts Discussed in Thread: TMS320DM368, TPS650061

您好,

TMS320DM368 Powering the TMS320DM368 with the TPS650061 中描述:

the device must be powered on in the following order:

1. 1.35V

2. 1.8V 

3. 3.3V

我们的DM368板子设计时没有考虑上电顺序问题,现在是同时上电,用sd卡启动时,经常卡死在准备引导内核的时候。但同一张sd卡在开发板上就能正常引导内核进入文件系统。

请问,这种卡死现象是否是因为上电顺序引起的,上电顺序不按照文档来的话还会有什么其他潜在问题,谢谢!

  • Lv Xianmin,

    可以同时上电,上电时序要求请参考最新的DM36x数据手册6.4.2 Restricted Power-On and Power-Off Method。

    请问你的DDR是否有根据你使用的DDR芯片修改相应的时序?是否有尝试过降低DDR频率,看问题是否能改善?

  • hi Chris:

    我们选型的DDR芯片和开发板上的DDR型号是一样的,我们也尝试过降低DDR频率,也存在这样的问题,每次卡死的地方还不一定,有时候在解压的时候卡死,有时候在文件系统那边卡死,我看了手册6.4.2 Restricted Power-On and Power-Off Method,是可以同时上电,但是也有条件,我们也有可能没有满足

    Steps 1, 2, and 3 may be performed simultaneously if the Main core finishes ramping up before the
    I/Os and the maximum delta voltage difference between the 1.8-V and 3.3-V I/Os is 2.0-V until the
    1.8-V I/O reaches the full voltage.

  • Lv Xianmin,

    请问你们板子的DDR布线是否有严格按照我们数据手册的要求来做?

    你降频时候DDR配置的是多少?

    kernel起来的时候,你是否有测量过电压,看是否在spec范围内?时钟是否都正常?

  • hi Chris:

    我们是按照DDR2标准的走线方式布的线,我降频的时候降到216Mhz

    测过电压,电压是正常,时钟也是对的,还有别的因素么?太奇怪了

  • hi Chris:

    还有一个问题,如果我DDR2 降频降到270M,能否支持1080P 30帧的编解码?