debug版本可以。用硬件仿真模式也可以。 就是release版本不可以。
中断函数的所有变量都定义成volatible类型了。
后面试了一下, 在main函数中循环发送一个字符, release版本也不成功
有人能给一些建议吗?
cmd文件如下:
-c
-heap 0x3000
-stack 0x3000
MEMORY
{
L1D: o = 00F00000h l = 00008000h
L1P: o = 00E00000h l = 00008000h
L2: o = 00800000h l = 00040000h
}
SECTIONS
{
.text > L2
.stack > L2
.bss > L2
.cinit > L2
.cio > L2
.const > L2
.sysmem > L2
.far > L2
.switch > L2
.data > L2
.vecs > L2
}
中断向量文件如下
.global _intcVectorTable
.global _c_int00
.global _vector1
.global _vector2
.global _vector3
.global _UART2_isr
.global _vector5
.global _vector6
.global _vector7
.global _vector8
.global _vector9
.global _vector10
.global _vector11
; This is a macro that instantiates one entry in the interrupt service table.
VEC_ENTRY .macro addr
STW B0,*--B15
MVKL addr,B0
MVKH addr,B0
B B0
LDW *B15++,B0
NOP 2
NOP
NOP
.endm
; This is a dummy interrupt service routine used to initialize the IST.
_vec_dummy:
B B3
NOP 5
; This is the actual interrupt service table (IST).
.sect ".vecs"
.align 1024
_intcVectorTable:
_vector0: VEC_ENTRY _c_int00 ;RESET
_vector1: VEC_ENTRY _vec_dummy ;NMI
_vector2: VEC_ENTRY _vec_dummy ;RSVD
_vector3: VEC_ENTRY _vec_dummy ;RSVD
_vector4: VEC_ENTRY _UART2_isr ;isr0
_vector5: VEC_ENTRY _vec_dummy ;isr0
_vector6: VEC_ENTRY _vec_dummy ;isr1
_vector7: VEC_ENTRY _vec_dummy ;isr2
_vector8: VEC_ENTRY _vec_dummy ;isr3
_vector9: VEC_ENTRY _vec_dummy
_vector10: VEC_ENTRY _vec_dummy
_vector11: VEC_ENTRY _vec_dummy
初始化程序
CSL_DspintcRegsOvly intcRegs = (CSL_DspintcRegsOvly)CSL_INTC_0_REGS;
uartRegs->PWREMU_MGMT = 0; // Reset UART TX & RX components
asm(" NOP 2");
uartRegs->FCR = 0x0001;
uartRegs->FCR = 0x0007; // Clear UART TX & RX FIFOs
asm(" NOP 2");
uartRegs->FCR = 0x0000; // Non-FIFO mode
uartRegs->LCR |=0x03; //b0,b1置1
uartRegs->MCR = 0x0000; // RTS & CTS disabled
uartRegs->MDR=1; //b0置1
uartRegs->DLL=136;
//uartRegs->DLH=0;
uartRegs->IER = 0x0005; // Enable interrupts
uartRegs->PWREMU_MGMT = 0xE001; // Enable TX & RX componenets
CSR&=0xfffe;//disable global interrupt
// connect the event to the interrupt 4
CSL_FINS(intcRegs->INTMUX1, DSPINTC_INTMUX1_INTSEL4, CSL_INTC_EVENTID_UARTINT1);
asm(" NOP 2");
// set ISTP to point to the vector table address
ISTP = (unsigned int)intcVectorTable;
asm(" NOP 2");
// clear all interrupts, bits 4 thru 15
ICR = 0xfff0;
asm(" NOP 2");
// b0 :reset b1:NMIE b4: INT4 enable the bits for non maskable interrupt and
IER=0x12; //
asm(" NOP 2");
// enable interrupts, set GIE bit
_enable_interrupts();