This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x仿真器XDS510V2连接出问题



在使用XDS510V2作为AM335x的仿真器时,连接时出现以下错误:

[Start]

Execute the command:

%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\DOCUME~1\ADMINI~1\LOCALS~1\APPLIC~1\.TI\
693494126\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100- or 510-class product.
This utility will load the adapter 'bhemujsc.dll'.
The library build date was 'Aug 20 2013'.
The library build time was '22:56:19'.
The library package version is '5.1.232.0'.
The library component version is '35.34.40.0'.
The controller does not use a programmable FPGA.

An error occurred while hard opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-115' (0xffffff8d).
The title is 'SC_ERR_OCS_PARM'.

The explanation is:
A bad parameter value passed to a function was detected.
The controller or software would later enter an invalid state.

[End]

请问一下这是什么原因呢?是不是该仿真器不只是AM335x系列的呢,只能使用XDS100?望解答,万分感谢!

  • 没用过这个型号,但是你可以看一下在配置文件中,这个型号是否有支持到AM335系列的下拉菜单。

    这里有篇trouble debugging guide,你可以根据自己的XDS510是Spectrum Digital,还是不是来跟进下一步:

    http://processors.wiki.ti.com/index.php/Debugging_JTAG_Connectivity_Problems#Host_connection_error