在使用XDS510V2作为AM335x的仿真器时,连接时出现以下错误:
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\DOCUME~1\ADMINI~1\LOCALS~1\APPLIC~1\.TI\
693494126\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'bhemujsc.dll'.
The library build date was 'Aug 20 2013'.
The library build time was '22:56:19'.
The library package version is '5.1.232.0'.
The library component version is '35.34.40.0'.
The controller does not use a programmable FPGA.
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-115' (0xffffff8d).
The title is 'SC_ERR_OCS_PARM'.
The explanation is:
A bad parameter value passed to a function was detected.
The controller or software would later enter an invalid state.
[End]
请问一下这是什么原因呢?是不是该仿真器不只是AM335x系列的呢,只能使用XDS100?望解答,万分感谢!