This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

5509A固化24flash不成功——续



软件:CCS6

芯片:5509A

flash:AT45DB161D-MU——SPI_24bit地址

现象:可以读出flash的ID,那么也说明可以向flash下载程序,即flash和dsp通信正常。

问题1:断电上电,不能从flash启动。bootmode正确。

问题2:如果BootLoader mode设置正确的话(设置从24bit flash启动),上电检测dsp的GPIO4,GPIO4脚电压是不是应该为高?