This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467 uart2数据发送不出去

DM6467 UART0/1功能都正常 

UART2 数据发送不出去,UTXD2量不到数据,

所以我们怀疑是pinmux问题,但是Pinmux配置为

PINMUX0 0x0 PINMUX1 0x15 VDD3P3V_PWDN 0x8000000

通过手册看PinMux也没有问题,gpio39和gpio40配置为utxd2和urxd2,同时无流控

同时写uart2的时候会出现too much work for irq42,所以感觉数据写到uart2的fifo里面了,数据没有往引脚去发送,导致一直触发中断,

在线等,急!