This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

对NandFlash烧写以后,再次想OMAPL138 仿真就不成功了



开发板开始是可以仿真的,我先用仿真器将ais程序烧写到了开发板,

烧写之后,代码没有运行成功,而且我想再次仿真时,就不能在仿真了,下面是结果
  
提示运行gel文件主要的错误

//DDR没有成功:
ARM9_0: Output:         PSC1 Sync Reset Transition Timeout on Domain 0, LPSC 6
ARM9_0: Output:         PSC1 Sync Reset Verify Timeout on Domain 0, LPSC 6

//DSP没有开启
ARM9_0: Output:         PSC0 Enable Core Transition Timeout on Domain 1, LPSC 15
ARM9_0: Output:         PSC0 Enable Core Verify Timeout on Domain 1, LPSC 15


如果我想再次通过仿真器烧写NandFlash,加载gel运行的结果还是这样的,然后我去load  "nand_write.out" 程序,然后程序就跑飞了,

请问各位大神是什么原因造成的,