你好,刚拿到手EVM5517开发板,用micro USB线缆连接EMU USB和电脑调试时报错 (在电脑设备管理器里可以看到已经有Spectrum digital tms320c5510 dsk设备驱动安装上了)。
报错内容如下
This error is generated by TI's USCIF driver or utilities.
The value is '-151' (0xffffff69).
The title is 'SC_ERR_FTDI_OPEN'.
The explanation is:
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
另外使用购买的仿真器用JTAG口是可以正常调试的。