This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM5517开发板板用micro USB线缆连接EMU USB和电脑调试时报错



你好,刚拿到手EVM5517开发板,用micro USB线缆连接EMU USB和电脑调试时报错 (在电脑设备管理器里可以看到已经有Spectrum digital tms320c5510 dsk设备驱动安装上了)。

报错内容如下 

This error is generated by TI's USCIF driver or utilities.

The value is '-151' (0xffffff69).
The title is 'SC_ERR_FTDI_OPEN'.

The explanation is:
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.

另外使用购买的仿真器用JTAG口是可以正常调试的。