This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error connecting to target:(Error - 2131 @ 0x0)

工程师您好,

    之前调试遇到类似问题,重启设备/CCS或重新插拔仿真器都可以解决,但这次一直都是这样的错误(如下图),请问有什么解决思路吗?

Test Connection之后打印如下:

[Start]

 

Execute the command:

 

%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

 

[Result]

 

 

-----[Print the board config pathname(s)]------------------------------------

 

C:\Users\zsy\AppData\Local\.TI\693494126\

    0\0\BrdDat\testBoard.dat

 

-----[Print the reset-command software log-file]-----------------------------

 

This utility has selected a 100- or 510-class product.

This utility will load the adapter 'seedjca8990isa.dll'.

The library build date was 'Apr  1 2013'.

The library build time was '23:55:08'.

The library package version is '5.1.73.0'.

The library component version is '35.34.40.0'.

The controller does not use a programmable FPGA.

The controller has a version number of '1' (0x00000001).

The controller has an insertion length of '16' (0x00000010).

This utility will attempt to reset the controller.

 

A error occurred while attempting to reset the controller.

 

-----[An error has occurred and this utility has aborted]--------------------

 

This error is generated by TI's USCIF driver or utilities.

 

The value is '-342' (0xfffffeaa).

The title is 'SC_ERR_HUNG_COMMAND'.

 

The explanation is:

Failure due to the controller command-finish taking too long.

 

[End]