工程师您好,
之前调试遇到类似问题,重启设备/CCS或重新插拔仿真器都可以解决,但这次一直都是这样的错误(如下图),请问有什么解决思路吗?
Test Connection之后打印如下:
|
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\zsy\AppData\Local\.TI\693494126\ 0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product. This utility will load the adapter 'seedjca8990isa.dll'. The library build date was 'Apr 1 2013'. The library build time was '23:55:08'. The library package version is '5.1.73.0'. The library component version is '35.34.40.0'. The controller does not use a programmable FPGA. The controller has a version number of '1' (0x00000001). The controller has an insertion length of '16' (0x00000010). This utility will attempt to reset the controller.
A error occurred while attempting to reset the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-342' (0xfffffeaa). The title is 'SC_ERR_HUNG_COMMAND'.
The explanation is: Failure due to the controller command-finish taking too long.
[End] |