This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X+TPS65910A3A1设计,PMIC_POWER_EN无法输出高电平?

Other Parts Discussed in Thread: TPS65910, TMDXEVM3358

大家好:

       如题,AM335X用TPS65910A3A1做电源芯片,有时PMIC_POWER_EN无法输出高电平。

      (1)能不能不用AM335X的PMIC_POWER_EN来控制TPS65910,TPS65910的PWRHOLD直接接VDDS_RTC(1.8V),TPS65910一上电就输出

               VDDS_RTC,直接使能电源芯片?

      (2)我看AM335X上电时序图,VDDS_RTC上电后,PMIC_POWER_EN会立即输出吗?RTC_PWRONRSTn的状态与PMIC_POWER_EN输出

               有什么关系?

       (3)我看AM335X_ICE_3h0013 BOARD 原理图,其中AM335X的RTC_PORZ(B5)接了一个100K的下拉电阻有什么作用吗?不接会怎样?

  • 建议你先读一下TPS65910的datasheet,明确TPS65910的上电使能所需要的方式。

    目前来说PMIC_POWER_EN来控制TPS5910不是唯一的途径,但是如果想一上电就输出是需要这样接的,这和TPS65910的设计相关,需要PMIC_POWER_EN来提供边沿触发以使能。参考电路,GPEVM板设计:http://www.ti.com/tool/tmdxevm3358

    另一种的使能方法,类似于我们的STARTERKIT EVM板,需要按住电源按键1S中,然后才可以使能上电,可以参考:http://www.ti.com.cn/tool/cn/tmdssk3358

  • 您好,感谢你的解答!

    我看过TPS65910上电使能的两种方式:1、通过PWRON,长按接地。2、通过PWRHOLD接AM335X的PMIC_POWER_EN
    来控制。我遇到的问题是上电时PMIC_POWER_EN没有输出使能信号(VDDS_RTC 1.8V输出正常),为了避免这种情况,能不能直接给TPS65910的PWRHOLD脚一直供1.8V的电压(VDDS_RTC),不用PMIC_POWER_EN来控制TPS65910使能?我不需要睡眠模式或低功耗模式。

  • 请参考附件的说明,要用TPS65910A31,而不是TPS65910A3A1

    swcu093c[2].pdf
  • 这两个到底有什么区别?我看数据手册时是同一份,VRTC驱动能力都是20mA,为什么TPS65910A3A1要外接Buck芯片,而TPS65910A31可以直接供电?

    这个表看不懂,盼解释!