This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

starterware的例程edmaTest.c , AM3358 的 EDMA 配置使用不了,求TI的大神帮忙看看哪里错误了!



本人使用starterware的库,配置EDMA,例子使用的是AM335X_StarterWare_02_00_01_01\examples\beaglebone\edma下面的edmaTest.c

裸机开发,例子的东西应该不会错的哇,但是又用不起来,我还有哪些地方没配置呢?或者遗漏哪里了呢/ 

代码的结果是:源数据跟目的数据不一样,目的数据没变化,也就是传输不成功!!!

代码进入到EDMAAppEDMA3Test()下面的这个末尾,也就是这个地方出错:

SrcBuff[index] != DstBuff[index

EDMA3Test: Data write-read matching FAILED.\r\n

具体代码如下:

main()

{

 MMUConfigAndEnable();

 CacheEnable(CACHE_ALL);

 //VFPv3Enable();

 EDMAModuleClkConfig();


/* Initialize EDMA */
EDMA3Init(EDMAAPP_EDMACC_BASE_ADDRESS, EDMAAPP_DMA_EVTQ);



/* Enable IRQ in CPSR. */
IntMasterIRQEnable();


/* Intialize ARM interrupt controller */
IntAINTCInit();


/* Registers Edma3ComplHandler0 Isr in Interrupt Vector Table of AINTC. */
IntRegister(SYS_INT_EDMACOMPINT , _EDMAAppEdma3ccComplIsr);


/* Set priority for system interrupt in AINTC */
IntPrioritySet(SYS_INT_EDMACOMPINT, 0u, AINTC_HOSTINT_ROUTE_IRQ);


/* Enable the EDMA CC0 system interrupt in AINTC.*/
IntSystemEnable(SYS_INT_EDMACOMPINT);


IntRegister(SYS_INT_EDMAERRINT , _EDMAAppEdma3ccErrIsr);


/* Set priority for system interrupt in AINTC */
IntPrioritySet(SYS_INT_EDMAERRINT, 0u, AINTC_HOSTINT_ROUTE_IRQ);


/* Enable the EDMA CCERR system interrupt AINTC.*/
IntSystemEnable(SYS_INT_EDMAERRINT);


#ifdef CH_TYPE_DMA
EDMAAppEDMA3Test();
#else
EDMAAppQDMA3Test();
#endif


EDMA3Deinit(EDMAAPP_EDMACC_BASE_ADDRESS, EDMAAPP_DMA_EVTQ);

}

具体的 EDMAAppEDMA3Test();如下: (都是直接复制edmaTest.c里面的函数!无改动)

void EDMAAppEDMA3Test()
{
volatile unsigned int index = 0u;
volatile unsigned int count = 0u;
EDMA3CCPaRAMEntry paramSet;
unsigned char data = 0u;
volatile unsigned int retVal = 0u;
unsigned int isTestPassed = false;
unsigned int numEnabled = 0u;
unsigned int aCount = EDMAAPP_MAX_ACOUNT;
unsigned int bCount = EDMAAPP_MAX_BCOUNT;
unsigned int cCount = EDMAAPP_MAX_CCOUNT;

/* Initalize source and destination buffers */
for (count = 0u; count < (aCount * bCount * cCount); count++)
{
SrcBuff[count] = data++;
/*
** No need to initialize the destination buffer as it is
** being invalidated.
*/
}

/* Request DMA channel and TCC */
retVal = EDMA3RequestChannel(EDMAAPP_EDMACC_BASE_ADDRESS,
                                                        EDMAAPP_DMA_CH_TYPE, EDMAAPP_DMA_CH_NUM,
                                                        EDMAAPP_DMA_TCC_NUM, EDMAAPP_DMA_EVTQ);

/* Registering Callback Function */
EDMAAppCallbackFxn[EDMAAPP_DMA_TCC_NUM] = &EDMAAppCallback;

if(TRUE == retVal)
{
/* Fill the PaRAM Set with transfer specific information */
paramSet.srcAddr = (unsigned int)(SrcBuff);
paramSet.destAddr = (unsigned int)(DstBuff);

paramSet.aCnt = (unsigned short)aCount;
paramSet.bCnt = (unsigned short)bCount;
paramSet.cCnt = (unsigned short)cCount;

/* Setting up the SRC/DES Index */
paramSet.srcBIdx = (short)aCount;
paramSet.destBIdx = (short)aCount;

if(EDMA3_SYNC_A == EDMAAPP_DMA_SYNC_TYPE)
{
/* A Sync Transfer Mode */
paramSet.srcCIdx = (short)aCount;
paramSet.destCIdx = (short)aCount;
}
else
{
/* AB Sync Transfer Mode */
paramSet.srcCIdx = ((short)aCount * (short)bCount);
paramSet.destCIdx = ((short)aCount * (short)bCount);
}

/* Configure the paramset with NULL link */
paramSet.linkAddr = (unsigned short)0xFFFFu;

paramSet.bCntReload = (unsigned short)0u;
paramSet.opt = 0u;

/* Src & Dest are in INCR modes */
paramSet.opt &= ~(EDMA3CC_OPT_SAM | EDMA3CC_OPT_DAM);

/* Program the TCC */
paramSet.opt |= ((EDMAAPP_DMA_TCC_NUM << EDMA3CC_OPT_TCC_SHIFT)
                              & EDMA3CC_OPT_TCC);

/* Enable Intermediate & Final transfer completion interrupt */
paramSet.opt |= (1u << EDMA3CC_OPT_ITCINTEN_SHIFT);
paramSet.opt |= (1u << EDMA3CC_OPT_TCINTEN_SHIFT);

if(EDMA3_SYNC_A == EDMAAPP_DMA_SYNC_TYPE)
{
paramSet.opt &= ~EDMA3CC_OPT_SYNCDIM;
}
else
{
/* AB Sync Transfer Mode */
paramSet.opt |= (1u << EDMA3CC_OPT_SYNCDIM_SHIFT);
}

/* Now, write the PaRAM Set. */
  EDMA3SetPaRAM(EDMAAPP_EDMACC_BASE_ADDRESS, EDMAAPP_DMA_CH_NUM,  &paramSet);

  EDMA3GetPaRAM(EDMAAPP_EDMACC_BASE_ADDRESS, EDMAAPP_DMA_CH_NUM,  &paramSet);
}

/*
** Since the transfer is going to happen in Manual mode of EDMA3
** operation, we have to 'Enable the Transfer' multiple times.
** Number of times depends upon the Mode (A/AB Sync)
** and the different counts.
*/
if(TRUE == retVal)
{
/* Need to activate next param */
if(EDMA3_SYNC_A == EDMAAPP_DMA_SYNC_TYPE)
{
numEnabled = bCount * cCount;
}
else
{
/* AB Sync Transfer Mode */
numEnabled = cCount;
}

for(index = 0u; index < numEnabled; index++)
{
IrqRaised = EDMAAPP_IRQ_STATUS_XFER_INPROG;

/*
** Now enable the transfer as many times as calculated above.
*/
retVal = EDMA3EnableTransfer(EDMAAPP_EDMACC_BASE_ADDRESS,
                                                    EDMAAPP_DMA_CH_NUM,
                                                    EDMAAPP_DMA_TRIG_MODE);

/* Wait for the Completion ISR. */
while(EDMAAPP_IRQ_STATUS_XFER_INPROG == IrqRaised)
{
/*
** Wait for the Completion ISR on Master Channel.
** You can insert your code here to do something
** meaningful.
*/
}

/* Check the status of the completed transfer */
if(IrqRaised < (int)EDMAAPP_IRQ_STATUS_XFER_INPROG)
{
/* Some error occured, break from the FOR loop. */
ConsoleUtilsPrintf("\r\nEDMA3Test: Event Miss Occured!!!\r\n");

/* Clear the error bits first */
EDMA3ClearErrorBits(EDMAAPP_EDMACC_BASE_ADDRESS,  EDMAAPP_DMA_CH_NUM, EDMAAPP_DMA_EVTQ);


break;
}
}
}

/* Match the Source and Destination Buffers. */
if(TRUE == retVal)
{
for(index = 0u; index < (aCount * bCount * cCount); index++)
{
if(SrcBuff[index] != DstBuff[index])
{
isTestPassed = false;
ConsoleUtilsPrintf("EDMA3Test: Data write-read matching FAILED.\r\n");
ConsoleUtilsPrintf("The mismatch happened at index : %d\r\n",
((int)index + 1u));
break;
}
}

if(index == (aCount * bCount * cCount))
{
isTestPassed = true;
ConsoleUtilsPrintf("EDMA3Test: Data write-read matching PASSED.\r\n");
}

/* Free the previously allocated channel. */
retVal = EDMA3FreeChannel(EDMAAPP_EDMACC_BASE_ADDRESS,
EDMAAPP_DMA_CH_TYPE, EDMAAPP_DMA_CH_NUM,
EDMAAPP_DMA_TRIG_MODE, EDMAAPP_DMA_TCC_NUM,
EDMAAPP_DMA_EVTQ);

/* Unregister Callback Function */
EDMAAppCallbackFxn[EDMAAPP_DMA_TCC_NUM] = NULL;

if(TRUE != retVal)
{
ConsoleUtilsPrintf("EDMA3Test: EDMA3_DRV_freeChannel() FAILED.\r\n");
}
}

if(true == isTestPassed)
{
ConsoleUtilsPrintf("EDMA3Test PASSED.\r\n");
}
else
{
ConsoleUtilsPrintf("EDMA3Test FAILED\r\n");
}
}

======================================================