This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467T的DSP核连不上仿真器



      dm6467t, CCS3.3,seed-xds560plus的仿真器,仿真器能连上arm核,dsp核连不上,报的错如下:

      “Error connecting to the target: Error 0x80001240/-121 Fatal Error during: Initialization, OCS, Target,  This error was generated by TI's USCIF driver.  SC_ERR_CMD_HANDLE <-121> A bad controller handle has been given to a function, either before attempting to open the controller, or after having opened the controller and ignored its error status. Valid controller handles are generated when attempts to open the controller return a clean error status.  ”

       连接arm的时候先加载evmdm6467_arm.gel(板子的gel的时钟和evm不一样,在gel里改成外部的了),然后连接arm核,然后再连接dsp核就报错了

       可能是什么原因呢 求助各位大侠了