dm6467t, CCS3.3,seed-xds560plus的仿真器,仿真器能连上arm核,dsp核连不上,报的错如下:
“Error connecting to the target: Error 0x80001240/-121 Fatal Error during: Initialization, OCS, Target, This error was generated by TI's USCIF driver. SC_ERR_CMD_HANDLE <-121> A bad controller handle has been given to a function, either before attempting to open the controller, or after having opened the controller and ignored its error status. Valid controller handles are generated when attempts to open the controller return a clean error status. ”
连接arm的时候先加载evmdm6467_arm.gel(板子的gel的时钟和evm不一样,在gel里改成外部的了),然后连接arm核,然后再连接dsp核就报错了
可能是什么原因呢 求助各位大侠了