This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EZDSP5515仿真器突然连接不上,上电引导还能用,怀疑是仿真芯片坏了,如果换一块的话,需要相应的XDS100V1 Emulator配置程序吧?



各位工程师,买的EZDSP5515仿真器突然连接不上,上电引导还能用,驱动卸了又装了,换了高版本的CCS,都不好用,test connectiom一直是

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

怀疑是仿真芯片坏了,如果换一块的话,需要相应的XDS100V1 Emulator配置程序吧?请问哪里有配置程序,要怎么用呢?

谢谢

  • 板子插到PC后,电脑能识别出板子吗?

    eZdsp上是xds100V2,你在配置文件里没选成xds100v1吧?

  • 你好,板子插上后,PC能识别出来

    ccxml文件,试了xds100v1和V2都不行。一直是这个错误

    -----[An error has occurred and this utility has aborted]--------------------

    This error is generated by TI's USCIF driver or utilities.

    The value is '-151' (0xffffff69).
    The title is 'SC_ERR_FTDI_OPEN'.

    The explanation is:
    One of the FTDI driver functions used during
    the connect returned bad status or an error.
    The cause may one or more of: invalid emulator serial number,
    blank emulator EEPROM, missing FTDI drivers, faulty USB cable.
    Use the xds100serial command-line utility in the 'common/uscif'
    folder to verify the emulator can be located.

    [End]

    仿真芯片摸起来有点热,应该是芯片烧了? 买一个新的换上能直接用吗?谢谢

  • 这个最好跟SDI公司确认一下。
    http://www.spectrumdigital.com/repairs-and-returns/