This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

8127 ipnc板检测不到nand



8127启动时,检测不到nand,以下为现象:

1)仿真器连接时,可烧写flash,由于烧进去的mlo可能有问题,无法通过nand启动

2)同样的代码,编译为通过串口引导,mlo可以起来,第二阶段无法检测到nand;编译为nand引导,通过仿真器烧录进去,第一阶段都起不来

3)flash的配置,是完全按照烧写程序nand-flash-writer.out代码里面的配置数据

问题:

除了nand gpmc的配置外,还有什么影响nand的检测,现在nand_get_flash_type函数中NAND_CMD_READID读出的数据连续4个都是3

  • 你好,

    bootmode引脚的上下拉是否配置正确?

  • 1)启动的问题:

    nand空的时候,串口可打出cccccc,应该是nand启动

    ccs调试,一直是停在串口打印信息那块

    void NS16550_putc (NS16550_t com_port, char c)
    {
    while ((serial_in(&com_port->lsr) & UART_LSR_THRE) == 0);//停在这里
    serial_out(c, &com_port->thr);
    }

    2)串口启动后,uboot检测问题

    在board_init函数里面增加了nand_pad_config_mux

    set_muxconf_regs();//按照模式1配置的gpmc D0-D16

    //nor_pad_config_mux();
    nand_pad_config_mux();//新增,类似 GPMC_D0, MODE(1) | INPUT_EN | PULL_DIS},内部的上下拉都未使用

    时钟是检测不出nand

  • 1)启动的问题:

    nand空的时候,串口可打出cccccc,应该是nand启动

    ccs调试,一直是停在串口打印信息那块

    void NS16550_putc (NS16550_t com_port, char c)
    {
    while ((serial_in(&com_port->lsr) & UART_LSR_THRE) == 0);//停在这里
    serial_out(c, &com_port->thr);
    }

    2)串口启动后,uboot检测问题

    在board_init函数里面增加了nand_pad_config_mux

    set_muxconf_regs();//按照模式1配置的gpmc D0-D16

    //nor_pad_config_mux();
    nand_pad_config_mux();//新增,类似 GPMC_D0, MODE(1) | INPUT_EN | PULL_DIS},内部的上下拉都未使用

    始终检测不出nand

  • 哦,自己有点东西搞错了

    中间加了些打印,nand启动时,串口还没初始化,打印就停在那里了

    还是原版程序,基本没动