各位:
DM8168 ddr的VTT为什么是接1.5V呢,谁能帮解释一下吗?图片见附件。
5V电源接到N36 N37,这个电源的上电顺序和其他有什么关系?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Shine Zhang 说:请看下面的FAQ.
Q:why is there a low impedance path between EVM_DDR_VTT and EVM_1V5?
A:"To keep VTT quiet and stable. The planar DDR3 boards work fine. The reason this is not on DIMM EVM is because VTT was moved to the DIMM."
意思是:EVM_DDR_VTT and EVM_1V5之间是低阻抗吗?
这句话没有理解:The reason this is not on DIMM EVM is because VTT was moved to the DIMM
感谢Shine Zhang的耐心解答。
Shine Zhang 说:1. EVM_DDR_VTT 和 EVM_1V5之间有个0.1uf的电容。
2. DIMM原理图如下,没用vtt。
http://support.spectrumdigital.com/boards/evm816xdimm/revc/files/evm816xdimm_Schematics_revc.pdf
首先感谢Shine Zhang的回答。
DIMM原理图中将内存放到内存条上(同时VTT也移到内存条上了),不过这好像和我的问题没有什么关系。
我想问的是为什么ddr的VTT通过电容接1.5V滤波。